TraceParts Help Center TraceParts Help Center
  • Deutsch
    • EnglishZu English wechseln
    • FrançaisZu Français wechseln
TraceParts Help Center TraceParts Help Center
TraceParts Help Center TraceParts Help Center
  • Deutsch
    • EnglishZu English wechseln
    • FrançaisZu Français wechseln
loading
  1. Home
  2. (3D Product Catalog Solutions) TraceParts Analytics
  3. Analyseansicht
  4. Inhalt einer Analyseansicht
  5. Tabelle
Aktualisiert am April 23, 2025
(3D Product Catalog Solutions) TraceParts Analytics
  • Schnittstelle
    • Menü
    • Sprache ändern
    • Sich abmelden
  • Analyseansicht
    • Dashboard
    • Inhalt einer Analyseansicht
      • Segment
      • Diagramme
      • Datumsauswahl
      • Kategorien
      • Tabelle
      • Handhabung von Daten
    • Gesamtansicht
    • Personalisierte Ansichten
  • Verwaltung
    • Dienstkonten
    • Benutzeraktivität
    • Benutzerverwaltung
      • Einen Benutzer einladen
      • Berechtigungen nach Rollen
  • Bericht
    • Download des Berichts
    • Planung
      • Zusammenfassung
      • Detaillierte Statistiken
      • Empfängerliste
  • Glossar
    • Glossar
  • Support kontaktieren

Tabelle

Voraussichtliche Lesedauer :2 minutes

The table is a detailed view that is displayed in the second part of the interface for an analytical view, regardless of the selected primary dimension.

Beschreibung der Vergleichstabelle

By default, the table always displays the list of the first 100 values.

The first column always shows the primary dimension (A).

Depending on what the user wishes to see, the second column may display the:

  • Metrics associated with the secondary dimension (B) if selected

    or

  • Metrics associated with the primary dimension (C); in the example above, it is the number of CAD file downloads

The following columns (respectively) show the:

  • Percentage represented by the metric of the primary dimension (D)
  • Metric of the primary dimension over the previous period (E)
  • Trend in the percentage of the metric compared to the previous period (F)

When the data comparison option is enabled, the previous period within the comparison column becomes the selected period.

The table display (default) can be replaced with one of the following displays.

When the table is replaced with one of the other charts available, a filter is applied to the top 10 for the purpose of making the data easier to read.

  • Bar chart (horizontal)
  • Bar chart (vertical)
  • Tree map
  • Pie chart

If the period comparison option is selected (see: data selector), each view will propose a model of the data over the required comparison period. In this case, to ensure that the data are easy to read, you are advised to reduce the number of segments displayed.

The „horizontal bar chart“ and „vertical bar chart“ can be used to view the data if the user has selected a secondary dimension.

The „tree map“ and „pie chart“ can also be used to select a secondary dimension, but it will not be displayed in the charts.

INHALTE